How to 'Clean Project'

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to 'Clean Project'

1,460件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri May 11 03:23:34 MST 2012
'Clean Project' is obviously 'Clean Build' = cleaning active Build (Debug or Release) :rolleyes:

Is there an option somewhere to clean my complete project (Debug & Release) or is this another wish-list issue?
0 件の賞賛
返信
2 返答(返信)

1,445件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri May 11 04:03:30 MST 2012

Quote: CodeRedSupport
A quick shortcut might be to just delete the Release and Debug directories from Project Explorer.



Good idea, I'll reprogram my backup program to do that for me :rolleyes:

Thanks for the hint :)
0 件の賞賛
返信

1,445件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri May 11 03:45:12 MST 2012
Hi Zero,

Sorry, but because of the way the build system works it is only possible to clean the active build configuration (which could be more than just Debug or Release). A quick shortcut might be to just delete the Release and Debug directories from Project Explorer.
0 件の賞賛
返信