Moving the Code from LPC1114 to LPC1115

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Moving the Code from LPC1114 to LPC1115

1,764件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by newpipe on Thu May 10 12:28:09 MST 2012
Hi!
I'm trying to port my project from the LPC1114 to our new LPC1115 because of the greater memory.
Are there any special things I have to consider?
I'm asking because I've already tried it, but after the initial flashing procedure I cannot erase or re flash the memory.
By the way, our project runs without any problems on the LPC1115, except that it seems to be locked after the initial flashing procedure.

Thanks in advance,
newpipe
1 返信

1,746件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kendwyer on Thu May 10 17:40:53 MST 2012
Check out this related blog:
http://www.microbuilder.eu/Blog.aspx
0 件の賞賛
返信