How Can I Clean Up Multiple LPXXpresso Setups?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How Can I Clean Up Multiple LPXXpresso Setups?

1,313件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Sep 27 00:43:46 MST 2013
I am on XP Pro SP3.

I have (currently) 5 or 6 installation of various flavours of the LPCXpresso IDE,
including Code Red v3, v5, and RedSuite; NXP v6. I have previously installed and
deleted (some) up to 15 various versions -- V4/V5/RedSuite/V6

It is claimed that the IDE setup does not use the registry (so I should be able to
simply delete the unwanted directories and desktop shortcuts).

BUT, what about the 'Start Menu' and registry 'Uninstall' Items? (I haven't looked yet).
ALSO 'Documents and Setings (all users)' has LPCXpresso, RedSuite5, and NXPLPCXpresso
folders (for the licences?). I'm guessing that I can delete a;; but NXPLPCXpresso?

A much bigger issue is the state of LPC-Link and LPC-Link2 driver stuff.
Even though I obly have ONE LPC-Link and ONE LPC-Link2 device, there are apparently
multiple device entries. [Text and html lists attached.]

Can you provide a tool to COMPLETELY remove all LPC-Link 1/2 from the system and the registry.
And then explain how to reinstall JUST the latest (IDE V6) driver WITHOUT having to reinstall
the V6 setup program.

Regards, Mike.

Original Attachment has been moved to: LPC-Link-List.html_.txt.zip

Original Attachment has been moved to: LPC-Link-List.txt.zip

0 件の賞賛
返信
4 返答(返信)

1,256件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 27 01:26:13 MST 2013
On Windows XP, the license files are stored in
%ALLUSERSPROFILE%
which is an environment variable whose value is typically "C:\Documents and Settings\All Users"`

The license files are stored in sub-directories:
[list]
  [*]Red Suite 5.x: RedSuite5
  [*]Red Suite 4.x: RedSuite
  [*]Red Suite 3.x: red_suite
  [*]LPCXpresso: LPCXpresso
[/list]

If you are not using the product, just delete the directory.
0 件の賞賛
返信

1,256件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Sep 27 01:13:09 MST 2013
Thanks for the hint.

I found these entried using UsbDViewf from nirsoft.net

Can you comment about the license files in Docs+Settings?

Cheers, Mike
0 件の賞賛
返信

1,256件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 27 01:05:43 MST 2013
After a bit of searching, I found this trick to show 'Hidden' devices in Device Manager
http://www.techrepublic.com/article/removing-unused-device-drivers-from-windows-xp-machines/

This provides a way to list 'unused' devices and to uninstall them.

Hope that helps
0 件の賞賛
返信

1,256件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 27 00:58:00 MST 2013
This is an artifact of Windows device drivers. They remain around because XP does not provide a convenient way of removing them (unlike Win7 etc, which does provide a convenient way of removing device drivers).

As you are using XP, I think you will either have to use a 3rd party tool to remove them, or you can try hand editing the registry (not recommended). Sorry,

Edit: BTW, they are benign. They are just occupying a bit of disk space.
0 件の賞賛
返信