HI!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HI!

714 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by erodrigues on Fri Aug 03 04:53:29 MST 2012
**** Build of configuration Debug for project CMSISv1p30_LPC11xx ****

make all
Building file: ../src/core_cm0.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -DDEBUG -D__CODE_RED -D__REDLIB__ -I"C:\Users\SAO\Documents\LPCXpresso_4.2.3_292\workspace4\CMSISv1p30_LPC11xx\inc" -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -v -mcpu=cortex-m0 -mthumb -MMD -MP -MF"src/core_cm0.d" -MT"src/core_cm0.d" -o"src/core_cm0.o" "../src/core_cm0.c"
Using built-in specs.
COLLECT_GCC=c:\nxp\LPCXpresso_4.2.3_292\lpcxpresso\tools\bin\arm-none-eabi-gcc.exe
Target: arm-none-eabi
Configured with: /var/code_red/builds/GNU/2010_100B/build/src/gcc-4.5-2010.09/configure --build=i686-pc-linux-gnu --host=i686-mingw32 --target=arm-none-eabi --enable-threads --disable-libmudflap --disable-libssp --disable-libstdcxx-pch --enable-extra-sgxxlite-multilibs --with-gnu-as --with-gnu-ld --with-specs='%{save-temps: -fverbose-asm} -D__CRT__RED_SUITE_MAJ__=2010 -D__CRT__RED_SUITE_MIN__=9 -D__CRT__RED_SUITE_REV__=51 %{O2:%{!fno-remove-local-statics: -fremove-local-statics}} %{O*:%{O|O0|O1|O2|Os:;:%{!fno-remove-local-statics: -fremove-local-statics}}}' --enable-languages=c,c++ --disable-shared --enable-lto --with-newlib --with-pkgversion='Red Suite 2010Q4 by Code Red' --with-bugurl=http://www.code-red-tech.com/support/bugs.html --disable-nls --prefix=/usr/opt/code_red --with-headers=yes --with-sysroot=/usr/opt/code_red/arm-none-eabi --with-build-sysroot=/var/code_red/builds/GNU/2010_100B/build/install/host-i686-mingw32/arm-none-eabi --with-libiconv-prefix=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-gmp=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-mpfr=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-mpc=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-ppl=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-host-libstdcxx='-static-libgcc -Wl,-Bstatic,-lstdc++,-Bdynamic -lm' --with-cloog=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-libelf=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --disable-libgomp --enable-poison-system-directories --with-build-time-tools=/var/code_red/builds/GNU/2010_100B/build/obj/tools-i686-pc-linux-gnu-2010.09-51-arm-none-eabi-i686-mingw32/arm-none-eabi/bin --with-build-time-tools=/var/code_red/builds/GNU/2010_100B/build/obj/tools-i686-pc-linux-gnu-2010.09-51-arm-none-eabi-i686-mingw32/arm-none-eabi/bin
Thread model: single
gcc version 4.5.1 (Red Suite 2010Q4 by Code Red)
COLLECT_GCC_OPTIONS='-DDEBUG' '-D__CODE_RED' '-D__REDLIB__' '-IC:\Users\SAO\Documents\LPCXpresso_4.2.3_292\workspace4\CMSISv1p30_LPC11xx\inc' '-O0' '-g3' '-Wall' '-c' '-fmessage-length=0' '-fno-builtin' '-ffunction-sections' '-v' '-mcpu=cortex-m0' '-mthumb' '-MMD' '-MP' '-MFsrc/core_cm0.d' '-MTsrc/core_cm0.d' '-o' 'src/core_cm0.o' '-D__CRT__RED_SUITE_MAJ__=2010' '-D__CRT__RED_SUITE_MIN__=9' '-D__CRT__RED_SUITE_REV__=51'
cc1 -quiet -v -IC:\Users\SAO\Documents\LPCXpresso_4.2.3_292\workspace4\CMSISv1p30_LPC11xx\inc -imultilib armv6-m -iprefix c:\progra~2\egcs\lib\gcc-lib\arm-none-eabi/4.5.1/ -isysroot c:\nxp\lpcxpresso_4.2.3_292\lpcxpresso\tools\bin\../arm-none-eabi -MMD src/core_cm0.d -MFsrc/core_cm0.d -MP -MTsrc/core_cm0.d -MQ src/core_cm0.o -dD -D__USES_INITFINI__ -DDEBUG -D__CODE_RED -D__REDLIB__ -D__CRT__RED_SUITE_MAJ__=2010 -D__CRT__RED_SUITE_MIN__=9 -D__CRT__RED_SUITE_REV__=51 ../src/core_cm0.c -quiet -dumpbase core_cm0.c -mcpu=cortex-m0 -mthumb -auxbase-strip src/core_cm0.o -g3 -O0 -Wall -version -fmessage-length=0 -fno-builtin -ffunction-sections -o C:\Users\SAO\AppData\Local\Temp\ccIjthKC.s
arm-none-eabi-gcc.exe: CreateProcess: No such file or directory
make: *** [src/core_cm0.o] Error 1
0 Kudos
Reply
2 Replies

697 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by erodrigues on Fri Aug 03 07:01:46 MST 2012
Hi Angelo!

I followed your  recomendation and checked the spaces in directories names. The directories are correct. The space was created when I imported the build log from LPCxpresso to the post.

Eduardo
0 Kudos
Reply

697 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Polux rsv on Fri Aug 03 05:13:02 MST 2012
Hi, too

If you read some older posts, you will discover that LPCxpresso, like many other toolchains, doesn't like spaces in directories names. Your "work space4" is probably the source of your problem.

edit: on another line, it is "works space4".

Angelo
0 Kudos
Reply