HI!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HI!

717 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by erodrigues on Fri Aug 03 04:53:29 MST 2012
**** Build of configuration Debug for project CMSISv1p30_LPC11xx ****

make all
Building file: ../src/core_cm0.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -DDEBUG -D__CODE_RED -D__REDLIB__ -I"C:\Users\SAO\Documents\LPCXpresso_4.2.3_292\workspace4\CMSISv1p30_LPC11xx\inc" -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -v -mcpu=cortex-m0 -mthumb -MMD -MP -MF"src/core_cm0.d" -MT"src/core_cm0.d" -o"src/core_cm0.o" "../src/core_cm0.c"
Using built-in specs.
COLLECT_GCC=c:\nxp\LPCXpresso_4.2.3_292\lpcxpresso\tools\bin\arm-none-eabi-gcc.exe
Target: arm-none-eabi
Configured with: /var/code_red/builds/GNU/2010_100B/build/src/gcc-4.5-2010.09/configure --build=i686-pc-linux-gnu --host=i686-mingw32 --target=arm-none-eabi --enable-threads --disable-libmudflap --disable-libssp --disable-libstdcxx-pch --enable-extra-sgxxlite-multilibs --with-gnu-as --with-gnu-ld --with-specs='%{save-temps: -fverbose-asm} -D__CRT__RED_SUITE_MAJ__=2010 -D__CRT__RED_SUITE_MIN__=9 -D__CRT__RED_SUITE_REV__=51 %{O2:%{!fno-remove-local-statics: -fremove-local-statics}} %{O*:%{O|O0|O1|O2|Os:;:%{!fno-remove-local-statics: -fremove-local-statics}}}' --enable-languages=c,c++ --disable-shared --enable-lto --with-newlib --with-pkgversion='Red Suite 2010Q4 by Code Red' --with-bugurl=http://www.code-red-tech.com/support/bugs.html --disable-nls --prefix=/usr/opt/code_red --with-headers=yes --with-sysroot=/usr/opt/code_red/arm-none-eabi --with-build-sysroot=/var/code_red/builds/GNU/2010_100B/build/install/host-i686-mingw32/arm-none-eabi --with-libiconv-prefix=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-gmp=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-mpfr=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-mpc=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-ppl=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-host-libstdcxx='-static-libgcc -Wl,-Bstatic,-lstdc++,-Bdynamic -lm' --with-cloog=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --with-libelf=/var/code_red/builds/GNU/2010_100B/build/obj/host-libs-2010.09-51-arm-none-eabi-i686-mingw32/usr --disable-libgomp --enable-poison-system-directories --with-build-time-tools=/var/code_red/builds/GNU/2010_100B/build/obj/tools-i686-pc-linux-gnu-2010.09-51-arm-none-eabi-i686-mingw32/arm-none-eabi/bin --with-build-time-tools=/var/code_red/builds/GNU/2010_100B/build/obj/tools-i686-pc-linux-gnu-2010.09-51-arm-none-eabi-i686-mingw32/arm-none-eabi/bin
Thread model: single
gcc version 4.5.1 (Red Suite 2010Q4 by Code Red)
COLLECT_GCC_OPTIONS='-DDEBUG' '-D__CODE_RED' '-D__REDLIB__' '-IC:\Users\SAO\Documents\LPCXpresso_4.2.3_292\workspace4\CMSISv1p30_LPC11xx\inc' '-O0' '-g3' '-Wall' '-c' '-fmessage-length=0' '-fno-builtin' '-ffunction-sections' '-v' '-mcpu=cortex-m0' '-mthumb' '-MMD' '-MP' '-MFsrc/core_cm0.d' '-MTsrc/core_cm0.d' '-o' 'src/core_cm0.o' '-D__CRT__RED_SUITE_MAJ__=2010' '-D__CRT__RED_SUITE_MIN__=9' '-D__CRT__RED_SUITE_REV__=51'
cc1 -quiet -v -IC:\Users\SAO\Documents\LPCXpresso_4.2.3_292\workspace4\CMSISv1p30_LPC11xx\inc -imultilib armv6-m -iprefix c:\progra~2\egcs\lib\gcc-lib\arm-none-eabi/4.5.1/ -isysroot c:\nxp\lpcxpresso_4.2.3_292\lpcxpresso\tools\bin\../arm-none-eabi -MMD src/core_cm0.d -MFsrc/core_cm0.d -MP -MTsrc/core_cm0.d -MQ src/core_cm0.o -dD -D__USES_INITFINI__ -DDEBUG -D__CODE_RED -D__REDLIB__ -D__CRT__RED_SUITE_MAJ__=2010 -D__CRT__RED_SUITE_MIN__=9 -D__CRT__RED_SUITE_REV__=51 ../src/core_cm0.c -quiet -dumpbase core_cm0.c -mcpu=cortex-m0 -mthumb -auxbase-strip src/core_cm0.o -g3 -O0 -Wall -version -fmessage-length=0 -fno-builtin -ffunction-sections -o C:\Users\SAO\AppData\Local\Temp\ccIjthKC.s
arm-none-eabi-gcc.exe: CreateProcess: No such file or directory
make: *** [src/core_cm0.o] Error 1
0 项奖励
回复
2 回复数

700 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by erodrigues on Fri Aug 03 07:01:46 MST 2012
Hi Angelo!

I followed your  recomendation and checked the spaces in directories names. The directories are correct. The space was created when I imported the build log from LPCxpresso to the post.

Eduardo
0 项奖励
回复

700 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Polux rsv on Fri Aug 03 05:13:02 MST 2012
Hi, too

If you read some older posts, you will discover that LPCxpresso, like many other toolchains, doesn't like spaces in directories names. Your "work space4" is probably the source of your problem.

edit: on another line, it is "works space4".

Angelo
0 项奖励
回复