GPIO 0_5 as out. IRQ problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPIO 0_5 as out. IRQ problem

800 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kisiel on Sun Feb 17 06:34:44 MST 2013
Hello,
I have already read topic about GPIO 0_5, open collector problem but I found new problem.
I connected LED to this pin to VCC.
I set pin 0_5 as GPIO as out put and value for output as "1' (led off)
I set up Timer CT16B0 for irq.
When irq is handled pin 0_5 goes down, and led is on. <deleted>
I think is great idea to make new blinky.asm src without touching io_pins .. word first? ;)
For me is hugh mistake and I really don't know what I can do with this error.
0 项奖励
回复
2 回复数

788 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kisiel on Sun Feb 17 09:46:42 MST 2013
LPC 1114 302, LPCXPRESSSO 5.0.19.
I use asm only in project to have best cycle exact application. I don't understand why irq state can change state of pinout.


PS. is this possible that .ltorg cause problems?
0 项奖励
回复

788 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Feb 17 07:19:17 MST 2013
:confused:

Which MCU and which software are we talking about :confused:
0 项奖励
回复