Fresh install - Cannot debug!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fresh install - Cannot debug!

2,392 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mitchsw on Tue Jul 24 23:18:16 MST 2012
Hi there,

I just purchased a LPC1114 LPCXpresso Board, followed the Getting Started guide closely, however I can't load blinky on to the board.

Error message at 57% when Launching blinky Debug:

Command failed: target extended-remote | crt_emu_lpc11_13_nxp -g -mi -2 -pLPC1114/302 -vendor=NXP -wire=hid -msg-port=1138

Reason:


There is no reason provided...

In the console, in red, is a single line:

set remotetimeout 60000


Searching hasn't returned much. Any ideas?

Cheers,
Mitch
0 Kudos
Reply
8 Replies

2,379 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mitchsw on Wed Jul 25 17:55:25 MST 2012
Indeed I can confirm a space anywhere in the install directory path breaks the IDE.

This should be fixed or warned about during install.

Mitch
0 Kudos
Reply

2,379 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mitchsw on Wed Jul 25 17:53:06 MST 2012
Fixed.

Following that lead, and reading this thread I changed my install directory from:

[INDENT]D:\Program Files\nxp\LPCXpresso_4.2.3_292\lpcxpresso[/INDENT]

to

[INDENT]D:\nxp\LPCXpresso_4.2.3_292\lpcxpresso[/INDENT]

and it worked fine.

Interestingly, D:\Program Files is not protected on my computer, which was the reason given in the previous thread. I suspect LPCXpresso has some issues with spaces in the directory name. A warning about this should be included...

Mitch
0 Kudos
Reply

2,379 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mitchsw on Wed Jul 25 17:44:31 MST 2012
Hi Angelo,

Unfortunately I have tried all the regular debug steps and have got no where here.

It might be worth mentioning when I launch LPCXpresso, whilst Loading Workbench the following error pops up:

Internal error: No vendors found
Exception


However pressing okay the program loads, and claims "LPCXpresso4 is fully activated".

Any ideas? Is there there a more official support avenue? Should I just return the damn thing?

Cheers,
Mitch
0 Kudos
Reply

2,379 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Polux rsv on Wed Jul 25 03:26:54 MST 2012
I also have a similar problem ( IDE stuck with "set remotetimeout 60000" message), but with a LPC1769 Xpresso board on Win7-64. Restarting and repluging everything solves the problem.
I didn't search any other solutions, or the root cause of this problem.

Angelo
0 Kudos
Reply

2,379 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mitchsw on Wed Jul 25 00:13:02 MST 2012
Hey,

1. Windows 7.
2. LPCXpresso v4.2.3_292.
3. Yes, no help.
4. Yes, no help.
5. Not sure what you mean here? How do I know?
6. Yes, activated.
7. Yes, LED is blinking.
8. No, there are no headers plugged in, powered from USB.

Thanks for your help.

Cheers,
Mitch
0 Kudos
Reply

2,379 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed Jul 25 00:03:51 MST 2012
So, lets try some standard questions that always get asked:

- which OS?
- whcih version of LPCXpresso?
- have you tried different USB ports
- have you got a proper USB2 cable?
- did LPC-Link boot?
- have you got a serial number and activated?
- if you just plug in LPCXpresso, does the LED flash?
- are you using a baseboard? Is it powered independently?
0 Kudos
Reply

2,379 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mitchsw on Tue Jul 24 23:50:31 MST 2012
I see no MCU Debug Log option on the console list, only C-Build and <terminated> blinky Debug
0 Kudos
Reply

2,379 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jul 24 23:41:26 MST 2012
What does the debug log say?
http://support.code-red-tech.com/CodeRedWiki/DebugLog
0 Kudos
Reply