Forgotten FMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Forgotten FMC

862件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Sep 06 05:14:26 MST 2012
@CodeRed:

I'm missing FMC registers in Peripherals (LPC11xx and LPC17xx) :confused:

Also FMC struct isn't included in LPC17xx.h :confused:
0 件の賞賛
返信
2 返答(返信)

847件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Sep 13 11:50:14 MST 2012
Sorry Zero - things are a bit hectic at the moment, and its easy to miss the odd post on the forum. Some of us don't live on here ;)

Anyway we'll do a bit of digging.

Regards,
CodeRedSupport
0 件の賞賛
返信

847件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Sep 13 09:05:26 MST 2012
... still missing some kind of answer...
0 件の賞賛
返信