External makefile project debugging problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External makefile project debugging problem

1,885件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ArtjomGromak on Fri Mar 02 15:32:24 MST 2012
Hi!
I use LPCXpresso for debug my program(as toolchain I use YAGARTO). But I want use LPCXpresso for editing and building too.
I import the existing project in IDE as Existing makefile project. Editing and build work. But I can't start debug. When I try create launch configuration LPCXpresso show message: No binaries found.
But elf (or axf) files exists.
[ATTACH]685[/ATTACH]
What I do wrong?

Thanks.
0 件の賞賛
返信
1 返信

1,702件の閲覧回数
maddin
Contributor I

I have exactly the same problem with MCUXpresso 10.1.1 606.

Can build the imported makefile project, axf exists but when try to create a launch configuration: "no binaries found.."

Any help would be appreciated. Thanks

0 件の賞賛
返信