External makefile project debugging problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External makefile project debugging problem

1,886 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ArtjomGromak on Fri Mar 02 15:32:24 MST 2012
Hi!
I use LPCXpresso for debug my program(as toolchain I use YAGARTO). But I want use LPCXpresso for editing and building too.
I import the existing project in IDE as Existing makefile project. Editing and build work. But I can't start debug. When I try create launch configuration LPCXpresso show message: No binaries found.
But elf (or axf) files exists.
[ATTACH]685[/ATTACH]
What I do wrong?

Thanks.
0 Kudos
Reply
1 Reply

1,703 Views
maddin
Contributor I

I have exactly the same problem with MCUXpresso 10.1.1 606.

Can build the imported makefile project, axf exists but when try to create a launch configuration: "no binaries found.."

Any help would be appreciated. Thanks

0 Kudos
Reply