Error while setting breakpoints

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error while setting breakpoints

720件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sharadanand on Mon Jan 09 22:18:50 MST 2012
I am using LPC1769 lpcpresso board with LPCXpresso IDE, my IDE is reporting error when I try put breakpoints at certain lines.
I am receiving following message

error reason:15 target error from register access

:(
0 件の賞賛
返信
1 返信

714件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jan 10 01:45:12 MST 2012
Please provide more information. For example
- are any breakpoints being set?
- what is different about the failing ones?
- is you target running or halted?
- how did you build you application?
- can you reproduce with one of the examples?
0 件の賞賛
返信