Element14 LPC4357 eval board example2 code for GPIO has incorrect comments

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Element14 LPC4357 eval board example2 code for GPIO has incorrect comments

522 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jcottier on Thu May 09 05:02:16 MST 2013
The code for GPIO blinky has incorrect comments on it which can lead to  utter confusion of how the GPIO and pin configuration works! :-


scu_pinmux(0xE ,7 , MD_PDN, FUNC4);     // P8.1 : USB0_IND1 LED

As per the Embset schematic, the LED is in fact connected to Pin PE.7, which is GPIO7.7 (GPIO = Function 4 on this pin).


Now, all the parameters make sense, and I still have some hair left.
0 项奖励
回复
0 回复数