Difference between NVIC and 8086 IV

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between NVIC and 8086 IV

1,909件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Fri May 06 20:15:43 MST 2011
Hello,

In the ARM world there are many strange acronyms for things that are natural in other microcontrollers.

One is "[B]NVIC[/B]".

[B]What is the difference between my old 8086 and Cortex-M0 or M3[/B] [B]?[/B]

It is not a comparison, but here I found a document explaining the operation.

Blogs/Webs recommendations that have tutorials on ARM (M0/M3) are welcome.

Thank you.
0 件の賞賛
返信
4 返答(返信)

1,838件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Sun May 08 11:36:43 MST 2011

Quote: Kartman
So exactly what is the issue?



Given much publicity, is sold as if it were the last Coca-Cola in the desert. lol


Quote: Kartman
The acronym forthecARM7 escapes me at the moment.



VECTORED INTERRUPT CONTROLLER (VIC).
0 件の賞賛
返信

1,838件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Kartman on Sun May 08 00:55:06 MST 2011
The ibm pc and most other 8088/8086 based computers used the Intel 8259 PIC. IV was the interrupt vector. In the Cortex world the NVIC is the nested vector interrupt Controller. The acronym forthecARM7 escapes me at the moment. I dont understand why you think it is strange - no stranger than the Z80 pio,dart and sio or the 6532 RIOT!
The cortex still has interrupt vectors and the NVIC is similar the the 8259 PIC. So exactly what is the issue?
0 件の賞賛
返信

1,838件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Fri May 06 23:08:42 MST 2011
Luis,  Bing or Google 8086 IVT, I got a bunch of hits.
0 件の賞賛
返信

1,838件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by atomicdog on Fri May 06 22:46:15 MST 2011

Quote: Luis Digital

[B]What is the difference between my old 8086 and Cortex-M0 or M3[/B] [B]?[/B]


About three decades. ;)


The ARM website has documents about migrating from different micro-processors to the ARM.
0 件の賞賛
返信