Debug problem LPC1769 Linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug problem LPC1769 Linux

1,001 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by FlySnake on Tue Jun 21 10:31:16 MST 2011
Hi all!
Please help me with a problem.
I'm trying to use LPCXpresso 1769 and Base Board from EmbeddedArtists. I've installed LPCXpresso IDE v3.8.3 on Linux openSUSE 11.2 (kernel 2.6.31.14-0.8-default). It runs OK, but I cannot debug any sample project. When I click on debug, it gives me error message:
Error launching Debug/demo.axf
putpkt: write failed: Broken pipe.:
But, I can flash the MCU by selecting "Binary Utilities / Program flash..." from context menu and it will work.
It looks like the known issue:

Quote:
LPCXpresso for Linux cannot connect to an RDB1768v2 board using the  built in debug connection unless the RDB1768v2 has been updated to the latest debug firmware. Note that updating the RDB1768v2 debug firmware is currently only possible under Windows.

But I'm not sure because I use another board and slightly different chip.
0 项奖励
回复
3 回复数

944 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by frame on Tue Jun 21 23:31:44 MST 2011
I have the same problem with two machines, one Suse11.2-x64 and one on Suse 11.0

However, I come so far only if I start the IDE as root. As normal user, it fails initializing the lpc-link with a timeout message (it fails to download the LPCXpressoWin.enc, because of access rights issues for /dev/usb).

The same board work under Windows, so it' neither a hardware issue nor a problem
of a specific Suse release.
0 项奖励
回复

944 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by FlySnake on Tue Jun 21 12:32:16 MST 2011
Just tried this on another PC with 11.4. Fail again, but now it said:
Error launching Debug/demo.axf
Remote communication error: connection reset by peer.:
I still can flash the program, but not debug it as in the first case.
Of course I can try Ubuntu if this is 100% distro's problem, but it's more likely I'm doing something wrong, not OS.
0 项奖励
回复

944 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Tue Jun 21 11:43:45 MST 2011
Hello,

Try updating your OpenSuse first, and then see this thread.
0 项奖励
回复