LPC1768 problem with pin P2.10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 problem with pin P2.10

1,100 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Michal on Sat Jul 07 06:28:31 MST 2012
Hello
I have soldered my LPC1768 on the board and the pin P2.10 is still on high level (3.3V). I checked the board and there is no mistake. I picked up new LPC1768 and I made connection test. The result is that P2.10 is connect to pin 96 (Vdd3.3V) and to pin P1.30. Is it ok? I can not use ISP bootloader becouse when I connect P2.10 to GND I have a short circuit:(
0 Kudos
Reply
3 Replies

997 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Michal on Sat Jul 07 08:10:39 MST 2012
I can not believe it! You are right :) Shame on my!
0 Kudos
Reply

997 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Sat Jul 07 07:07:38 MST 2012
The first time, I too made the same mistake. lol
0 Kudos
Reply

997 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Jul 07 06:54:55 MST 2012
I guess it is the first time you are soldering LPC1768 ;)

What you are describing sounds like as you have mixed up pin1 :eek:

Described in http://knowledgebase.nxp.com/showthread.php?p=14562&langid=1

Picture: http://flic.kr/p/bxSbea
0 Kudos
Reply