Debug button off

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug button off

876件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Thu May 12 00:11:24 MST 2016
LPCXpresso v8.1.4 [Build 606] [2016-03-14]
LPC1758
LPCLink

Yesterday everything worked well, this morning however after connecting with LPCLink the play buttons, steps are not active !!
The LPCLink connects properly, the green line is in the mai first line, but the debug button is off !!

What may have happened ?

Thanks
0 件の賞賛
返信
2 返答(返信)

785件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

785件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Fri May 13 02:33:06 MST 2016
After many test . . . solved the problem changing the prospecrive from debug to develop and then restart the lpcxpresso application.
0 件の賞賛
返信