Debug button off

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug button off

910 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Thu May 12 00:11:24 MST 2016
LPCXpresso v8.1.4 [Build 606] [2016-03-14]
LPC1758
LPCLink

Yesterday everything worked well, this morning however after connecting with LPCLink the play buttons, steps are not active !!
The LPCLink connects properly, the green line is in the mai first line, but the debug button is off !!

What may have happened ?

Thanks
0 项奖励
回复
2 回复数

819 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复

819 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Fri May 13 02:33:06 MST 2016
After many test . . . solved the problem changing the prospecrive from debug to develop and then restart the lpcxpresso application.
0 项奖励
回复