Debug Problem - Can´t Restart

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug Problem - Can´t Restart

3,912件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Fernando on Thu Dec 30 15:41:46 MST 2010
Hello, I´m having a problem with the Debug mode.
As you can see in the picture, i cant restart the execution of the code.
This is something that has happened a couple of times before but randomly.
I also wasnt able to add global variables, but I fixed it by closing the "variables" view and opening it again.

Best regards,
Fernando
0 件の賞賛
返信
14 返答(返信)

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri May 27 03:20:42 MST 2011
Which OS are you running?

Did you try to work with an original LPCXpresso board?

Does this problem occur if you start a new LPCXpresso project?

If so, please post it (LPC1114).
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by plebi on Fri May 27 02:10:42 MST 2011
I use LPC1752 and LPC1114 and on both no 'RESTART'.

Connection from LPCXpresso board to my board:
- VIO_3V3
- SWDIO
- SWCLK
- RESET
- GND
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu May 26 07:00:46 MST 2011
Which MCU are you using and which SWD-wires did you connect?
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by plebi on Thu May 26 06:54:56 MST 2011
LPCXpresso is used to programm and debug my own board.
Programming, degugging, breakpoints works well - only restart didnt work.
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu May 26 06:36:24 MST 2011
Are you using your own board or LPCXpresso?
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by plebi on Thu May 26 06:22:04 MST 2011
Ive installed a newest version of LPC and after that restarted PC.
Restart button still is inactive :-(
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by plebi on Thu May 26 03:02:12 MST 2011
Ok. I'll try.
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu May 26 02:25:41 MST 2011
Why don't you update to 3.6.3 / 317 and hope that your problem disappears :)
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by plebi on Thu May 26 02:21:47 MST 2011
unfortunately no :-(
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Thu May 26 01:52:34 MST 2011
If you pause the debugger does the restart icon become active?
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by plebi on Thu May 26 01:36:33 MST 2011
Im using LPCXpresso 3.6.2 [Build 279] [29/01/2011]  on two computers and on both I cant use 'restart' button also.  It's still inactive.
On one computer button was active and worked well but only one day after upgrade LPCX (I dont remember if whole day).
After that day still is inactive. To restart debugger I should programm uC again.
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Fernando on Fri Dec 31 04:14:52 MST 2010
I upgraded the IDE and it´s working now.
Thanks again.

Best regards,
Fernando.
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Fernando on Fri Dec 31 03:51:24 MST 2010
As I mentioned in the previous post, it had happened in the past but i was able then to restart the debug.
What is happening now is that I´m not able to restart debug since yesterday, and i´ve tried a lot of times.
The version I´m using is V3.3.4 and I  don´t have any breakpoint set.
I will try upgrading the IDE.

Thanks for your fast response.

Best regards,
Fernando.
0 件の賞賛
返信

3,899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Dec 31 01:03:43 MST 2010
Are you saying that you now never have the restart icon available, or is this just something that happens occasionally? If it is only occasional, can you narrow down the circumstances in which you see it. For example, if you set a breakpoint on the particular line, does it always occur? Or is it just if you select the pause icon?

Can you confirm what version of LPCXPresso IDE you are using. From your screenshot it appears that you may be using version 3.3.x.

Can I suggest that you try upgrading to the latest version (3.6.0) and see if you continue to see the same problems?

Regards,
CodeRedSupport.
0 件の賞賛
返信