lpcxpresso 3.6 not recognizing SSP1 on 1113/301

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpcxpresso 3.6 not recognizing SSP1 on 1113/301

530 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by smichaud on Tue Dec 28 15:20:58 MST 2010
I just downloaded lpcxpresso version v3.6.0, and tried out my existing code (which runs fine on version v3.5.0), and it looks like SSP1 is somehow not being recognized.

I am running on an LPC113F/301 processor - I checked, and that processor is (still) selected by my project, under Project Properties / C/C++ Build / MCU Settings.

The code does compile and download, but the debugger (Peripheral Registers) no longer shows an entry for SSP0

Is this a know problem, or something I can fix with a file edit somewhere in the lpcxpresso v3.6.0 directories?  Could I be missing something in my configuration somewhere?  Or do I need to roll back to v3.5.0 and wait for a fix..?

Thanks,     Sean

Original Attachment has been moved to: 1100929_log.zip

0 Kudos
Reply
2 Replies

455 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by smichaud on Wed Dec 29 09:37:00 MST 2010
Great, thanks guys, that did the trick -

Sean
0 Kudos
Reply

455 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Dec 29 03:51:34 MST 2010
Yes, I can replicate this here. We will investigate fixing in the next release of LPCXpresso.

As a workaround for now, try placing the nxp_lpc11xx.xme file from the attached ZIP file into the bin subdirectory of your LPCXpresso 3.6.0 installation (back up the original xme file first). This should give you visibility of SSP1 in the peripheral view.

[Note that this file will only work with LPCXpresso, not with RedSuite or RedSuite NXP edition.]

Regards,
CodeRedSupport
0 Kudos
Reply