Code red support for LPC1227

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code red support for LPC1227

1,047 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by opprud on Sun Jul 10 01:49:10 MST 2011
Hi,

Are you planning a soon release of code examples for the lpc1227 device, on the lpcXpresso board.

We are currently planning a design using the lpc1227, and therefore any examples, similar to those provided with the lpc1114 board, would be much appreciated. This would ease the prototype devlopment a lot. otherwise we might consider another device with more SW support.

best regards
Morten Opprud
0 Kudos
Reply
3 Replies

1,021 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Sun Jul 10 04:02:46 MST 2011

Quote:
Wow :eek: Or consider to hire a SW engineer :confused:


I'm, still available, Århus is not that far away from the Netherlands :D
I have > 20 years experience in ARM programming of which 10 years with microcontroller based on ARM cores.

Regards,

Rob
0 Kudos
Reply

1,021 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by opprud on Sun Jul 10 02:46:18 MST 2011
found the examples in the release 4 ;-)
The device is not critical yet, so for the prototype we will mount what can get us ahead fastest (= suited device with mos example code...)
0 Kudos
Reply

1,021 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Jul 10 01:59:38 MST 2011

Quote: opprud
Are you planning a soon release of code examples for the lpc1227 device, on the lpcXpresso board.




Done in Example Folder :)


Quote: opprud
otherwise we might consider another device with more SW support



Wow :eek: Or consider to hire a SW engineer :confused:
0 Kudos
Reply