Code-Red Support Website: Forbidden page

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code-Red Support Website: Forbidden page

1,086 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Mon Sep 17 00:59:04 MST 2012
[SIZE=2][FONT=Tahoma]On the CodeRed support wiki site, I did a text search for "Debug".

One entry one the result page was "[/FONT][/SIZE][FONT=Tahoma][SIZE=2]Setting the crystal and PLL for a target board"; which sounds interresting.

However, clicking the link opens a page with "[/SIZE][/FONT][B][FONT=Tahoma][SIZE=2][B]You are not allowed to view this page.[/B][/SIZE][/FONT][/B][FONT=Tahoma][SIZE=2]". :confused::(:eek:

What's going on? Why am I not able to view the page? (I was logged on.) Is there any special (additional) registration options of which I am not aware? Or is this a website error?

If this is [I]not[/I] an accessible page, surely it should [I]not[/I] show up from the search.

The actual link is [/SIZE][/FONT][FONT=Tahoma][SIZE=1]http://support.code-red-tech.com/CodeRedWiki/CrystalAndPLL

[SIZE=2]Please CodeRed, solve this enigma for me.
Regards.[/SIZE]
[/SIZE][/FONT]
0 Kudos
Reply
2 Replies

1,074 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Mon Sep 17 04:29:04 MST 2012
[SIZE=2][FONT=Tahoma]Amazing response time! c.a. three and a half hours. Including a fix.
Thanks.:)
[/FONT][/SIZE]
0 Kudos
Reply

1,074 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Sep 17 04:23:46 MST 2012
Thanks for the report. There was an access permission issue with that page. Now fixed.

Note that if you want to look at Debug related FAQs, I would suggest in the first place browsing the "Debug" and "Debug target connections" sections of:

http://support.code-red-tech.com/CodeRedWiki/CodeRedFAQ

or directly:
http://support.code-red-tech.com/CodeRedWiki/CodeRedFAQ#Debug
http://support.code-red-tech.com/CodeRedWiki/CodeRedFAQ#DebugConnection

And for searching, I would recommend using:

http://support.code-red-tech.com/CodeRedWiki/SearchPage

Regards,
CodeRedSupport
0 Kudos
Reply