CRP problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CRP problem

770件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Thu Jul 07 07:53:15 MST 2011
LPC1758
I use LPCLINK, "programm flash" buton, and the same hex file.
When I program the flash without any CRP, all goes correctly, the application run.
When I program the flash with CRP1, the application dont start !!!

Can help me ?
0 件の賞賛
返信
1 返信

755件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Fri Jul 08 11:55:20 MST 2011
Please see application note below:

http://ics.nxp.com/support/documents/microcontrollers/zip/an10851.zip

Keep in mind that debug capability is lost after CRP1 is enabled.
Thanks.
0 件の賞賛
返信