CRP problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CRP problem

768 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Thu Jul 07 07:53:15 MST 2011
LPC1758
I use LPCLINK, "programm flash" buton, and the same hex file.
When I program the flash without any CRP, all goes correctly, the application run.
When I program the flash with CRP1, the application dont start !!!

Can help me ?
0 项奖励
回复
1 回复

753 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Fri Jul 08 11:55:20 MST 2011
Please see application note below:

http://ics.nxp.com/support/documents/microcontrollers/zip/an10851.zip

Keep in mind that debug capability is lost after CRP1 is enabled.
Thanks.
0 项奖励
回复