CRP problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CRP problem

779 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Thu Jul 07 07:53:15 MST 2011
LPC1758
I use LPCLINK, "programm flash" buton, and the same hex file.
When I program the flash without any CRP, all goes correctly, the application run.
When I program the flash with CRP1, the application dont start !!!

Can help me ?
0 Kudos
Reply
1 Reply

764 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Fri Jul 08 11:55:20 MST 2011
Please see application note below:

http://ics.nxp.com/support/documents/microcontrollers/zip/an10851.zip

Keep in mind that debug capability is lost after CRP1 is enabled.
Thanks.
0 Kudos
Reply