CMSIS DAP vs Redlink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS DAP vs Redlink

2,304件の閲覧回数
vojtechhavlicek
Contributor III

I would like to ask what is better choice for debugging - CMSIS DAP or Redlink image for LPC-Link 2? I use LPCXpresso 8.1.4 and I´ve bought LPC-Link 2. I use LPC812, LPC824, LPC4310.

 

Are there any major differences?

 

Thanks

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,831件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,831件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Only CMSIS-DAP firmware is now supported in recent LPCXpresso IDE releases. But you still connect through what was called Redlink Server on your host PC, now known as LinkServer.

There is a bit more information on this at

What is Redlink?

Configuring which LPC-Link2 firmware image to soft-load

Regards,

LPCXpresso Support

0 件の賞賛
返信