CMSIS DAP vs Redlink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CMSIS DAP vs Redlink

2,312 Views
vojtechhavlicek
Contributor III

I would like to ask what is better choice for debugging - CMSIS DAP or Redlink image for LPC-Link 2? I use LPCXpresso 8.1.4 and I´ve bought LPC-Link 2. I use LPC812, LPC824, LPC4310.

 

Are there any major differences?

 

Thanks

0 Kudos
Reply
2 Replies

1,839 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,839 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Only CMSIS-DAP firmware is now supported in recent LPCXpresso IDE releases. But you still connect through what was called Redlink Server on your host PC, now known as LinkServer.

There is a bit more information on this at

What is Redlink?

Configuring which LPC-Link2 firmware image to soft-load

Regards,

LPCXpresso Support

0 Kudos
Reply