CAN channels accessible

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN channels accessible

893 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jlara on Wed Oct 20 19:31:02 MST 2010
I just purchased the LPCxpresso for the 1768.  I did not see more than one CAN channel accessible on the board.  This micro has two CAN channels.  Is it possible to use the other channel? 

Also, the board came with a 'Coupon Code'.  Is this code used for anything?

Thanks!
0 项奖励
回复
2 回复数

879 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jlara on Sat Oct 23 19:13:18 MST 2010
Thanks, Zero!

I appreciate the help very much.
0 项奖励
回复

879 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Oct 20 20:48:56 MST 2010
Of course LPC1768 has 2 CAN channels :D.

Although

http://www.embeddedartists.com/products/lpcxpresso/LPCXpressoLPC1768revA.pdf

Page 7 only describes CAN Channel 2, Channel 1 can be used via P0[0] & P0[1] (see User Manual).



Quote:
[SIZE=3][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00]When you buy an LPCXpresso board you will receive a unique coupon code printed on the flyer received together with the board. Using this code in Embedded Artists’ web shop gives you [/FONT][/SIZE][/FONT][/SIZE][FONT=TTFF5AA840t00][SIZE=3][FONT=TTFF5AA840t00][SIZE=3]15 EUR [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00][SIZE=3]discount on Embedded Artists’ regular [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5AA840t00][SIZE=3][FONT=TTFF5AA840t00][SIZE=3]Developer’s Kits [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00][SIZE=3]see: [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5A8290t00][SIZE=3][COLOR=#336689][FONT=TTFF5A8290t00][SIZE=3][COLOR=#336689][FONT=TTFF5A8290t00][SIZE=3][COLOR=#336689]http://www.embeddedartists.com/products/kits/ [/COLOR][/SIZE][/FONT][/COLOR][/SIZE][/FONT][/COLOR][/SIZE][/FONT][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00][SIZE=3].[/SIZE][/FONT][/SIZE][/FONT]
[SIZE=3][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00]The coupon code also gives you 7[/FONT][/SIZE][/FONT][/SIZE][FONT=TTFF5AA840t00][SIZE=3][FONT=TTFF5AA840t00][SIZE=3] EUR [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00][SIZE=3]off the [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5AA840t00][SIZE=3][FONT=TTFF5AA840t00][SIZE=3]LPCXpresso Base board.[/SIZE][/FONT][/SIZE][/FONT]



see


[LEFT]http://www.embeddedartists.com/products/lpcxpresso/LPCXpresso_Discount.pdf
[/LEFT]
0 项奖励
回复