CAN channels accessible

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN channels accessible

913件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jlara on Wed Oct 20 19:31:02 MST 2010
I just purchased the LPCxpresso for the 1768.  I did not see more than one CAN channel accessible on the board.  This micro has two CAN channels.  Is it possible to use the other channel? 

Also, the board came with a 'Coupon Code'.  Is this code used for anything?

Thanks!
0 件の賞賛
返信
2 返答(返信)

899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jlara on Sat Oct 23 19:13:18 MST 2010
Thanks, Zero!

I appreciate the help very much.
0 件の賞賛
返信

899件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Oct 20 20:48:56 MST 2010
Of course LPC1768 has 2 CAN channels :D.

Although

http://www.embeddedartists.com/products/lpcxpresso/LPCXpressoLPC1768revA.pdf

Page 7 only describes CAN Channel 2, Channel 1 can be used via P0[0] & P0[1] (see User Manual).



Quote:
[SIZE=3][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00]When you buy an LPCXpresso board you will receive a unique coupon code printed on the flyer received together with the board. Using this code in Embedded Artists’ web shop gives you [/FONT][/SIZE][/FONT][/SIZE][FONT=TTFF5AA840t00][SIZE=3][FONT=TTFF5AA840t00][SIZE=3]15 EUR [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00][SIZE=3]discount on Embedded Artists’ regular [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5AA840t00][SIZE=3][FONT=TTFF5AA840t00][SIZE=3]Developer’s Kits [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00][SIZE=3]see: [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5A8290t00][SIZE=3][COLOR=#336689][FONT=TTFF5A8290t00][SIZE=3][COLOR=#336689][FONT=TTFF5A8290t00][SIZE=3][COLOR=#336689]http://www.embeddedartists.com/products/kits/ [/COLOR][/SIZE][/FONT][/COLOR][/SIZE][/FONT][/COLOR][/SIZE][/FONT][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00][SIZE=3].[/SIZE][/FONT][/SIZE][/FONT]
[SIZE=3][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00]The coupon code also gives you 7[/FONT][/SIZE][/FONT][/SIZE][FONT=TTFF5AA840t00][SIZE=3][FONT=TTFF5AA840t00][SIZE=3] EUR [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5A8290t00][SIZE=3][FONT=TTFF5A8290t00][SIZE=3]off the [/SIZE][/FONT][/SIZE][/FONT][FONT=TTFF5AA840t00][SIZE=3][FONT=TTFF5AA840t00][SIZE=3]LPCXpresso Base board.[/SIZE][/FONT][/SIZE][/FONT]



see


[LEFT]http://www.embeddedartists.com/products/lpcxpresso/LPCXpresso_Discount.pdf
[/LEFT]
0 件の賞賛
返信