C Project vs LPCxpresso C Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

C Project vs LPCxpresso C Project

725 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bilgehanparay on Thu Mar 05 05:08:43 MST 2015
Sorry guys if this is in the user guide.(I could not find it.)

[img]http://imgim.com/5781incig5223974.png[/img]

What is the difference between C project and LPCxpresso C project? Which one should I choose to program lps812 tssop 20 mcu. (no boards)

Also, is there a way to test-debug the code without having the mcu?

0 Kudos
Reply
1 Reply

669 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Mar 05 05:35:36 MST 2015
For LPCXpresso projects, use LPCXpresso C Project... The "C Project" can be used for creating 'native' projects for running on the host (Windows, Linux etc), and so does not configure the MCU type or setup the correct tool settings.

Note that if you use the "Quickstart->New Project" button it will automatically create the correct type.
0 Kudos
Reply