C Project vs LPCxpresso C Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

C Project vs LPCxpresso C Project

728件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bilgehanparay on Thu Mar 05 05:08:43 MST 2015
Sorry guys if this is in the user guide.(I could not find it.)

[img]http://imgim.com/5781incig5223974.png[/img]

What is the difference between C project and LPCxpresso C project? Which one should I choose to program lps812 tssop 20 mcu. (no boards)

Also, is there a way to test-debug the code without having the mcu?

0 件の賞賛
返信
1 返信

672件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Mar 05 05:35:36 MST 2015
For LPCXpresso projects, use LPCXpresso C Project... The "C Project" can be used for creating 'native' projects for running on the host (Windows, Linux etc), and so does not configure the MCU type or setup the correct tool settings.

Note that if you use the "Quickstart->New Project" button it will automatically create the correct type.
0 件の賞賛
返信