Build problems with v3.6.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build problems with v3.6.2

931件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Tue Feb 08 11:58:22 MST 2011
I've just installed v3.6.2 and am having build problems:


**** Build of configuration Debug for project LPCXpresso1343_blinky ****

make all
m.AllocationBase 0x0, m.BaseAddress 0x71110000, m.RegionSize 0x50000, m.State 0x10000
C:\NXP\lpcxpresso_3.6.2\msys\bin\sh.exe: *** Couldn't reserve space for cygwin's heap (0x71110000 <0x24A0000>) in child, Win32 error 0
make: *** [src/blinky.o] Error 1

The previous version worked OK.

I'm using Win7 x64.

Leon
0 件の賞賛
返信
2 返答(返信)

914件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Tue Feb 08 12:34:05 MST 2011
Thanks. That seems to have fixed the problem.
0 件の賞賛
返信

914件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Feb 08 12:11:09 MST 2011
http://support.code-red-tech.com/CodeRedWiki/VirtualAllocPointerNull
0 件の賞賛
返信