Breakpoint attribute problem: installation failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Breakpoint attribute problem: installation failed

2,226件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Thu Nov 22 22:16:04 MST 2012
Hi

This problem started suddenly from one debug session to another:

[I][B]Breakpoint attribute problem: installation failed[/B][/I]


I cannot set breakpoints, although I've been working only with the "debug" release.

It seems to be a problem in the Eclipse's latest release, Indigo. And it also seems to be not fixed so far.

Any ideas?
0 件の賞賛
返信
3 返答(返信)

1,667件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sun Nov 25 03:30:56 MST 2012

Quote: fjrg76
Hi


This is known problem. The first time it was showed I googled it and I found some workarounds:

Google: Breakpoint attribute problem: installation failed
Aproximadamente 361,000 resultados (0.16 segundos)




It is a known *error message*, but not a known *problem*. From looking through the top hits, AFAICT, they were all due to user misunderstandings, or user error. I can't see ANY that are due to an error in Eclipse.
0 件の賞賛
返信

1,667件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Sat Nov 24 22:00:31 MST 2012
Hi

I'll wait for the problem to show itself again so I can ask all your questions. Meanswhile:


Quote: CodeRedSupport
This is not a known problem. Can you please tell try removing ALL breakpoints in the Breakpoint view, and then recreating them.



This is known problem. The first time it was showed I googled it and I found some workarounds:

Google: Breakpoint attribute problem: installation failed
Aproximadamente 361,000 resultados (0.16 segundos)


Quote:

If this does not help, please try to provide as much information as possible on how to reproduce. For example
- how are you building your application? Are you using Debug or Release?



I was using "Debug"


Quote:

- In your workspace, do you have several files with the same name?



Just one main.c


Quote:

- How are you setting the breakpoints?



Double click in the left margin of the source editor.


Quote:

- Can you post the contents of the 'gdb traces' Console?



ASAP the problem shows up I'll do it, and also I'll try to send you all the information I can gather.


Quote:

BTW: The latest release of Eclipse is Juno (not Indigo) and LPCXpresso v5 is based on Juno.



My mistake :D
0 件の賞賛
返信

1,667件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Nov 23 02:24:20 MST 2012
This is not a known problem. Can you please tell try removing ALL breakpoints in the Breakpoint view, and then recreating them.

If this does not help, please try to provide as much information as possible on how to reproduce. For example
- how are you building your application? Are you using Debug or Release?
- In your workspace, do you have several files with the same name?
- How are you setting the breakpoints?
- Can you post the contents of the 'gdb traces' Console?

BTW: The latest release of Eclipse is Juno (not Indigo) and LPCXpresso v5 is based on Juno.
0 件の賞賛
返信