Another toolchain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Another toolchain

969 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SebastianKulik on Sun Jun 27 02:25:00 MST 2010
hi@all

Im hardware developer and learn programming for myself.
My goal is intelligent MIDI things.

Would LPCXpresso work with another IDE (Keil, IAR, etc)?

THX,
Sebastian
0 Kudos
Reply
2 Replies

961 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jun 28 09:58:19 MST 2010
Hi Sebastian,

if you look for an easy entry, I would suggest to start with LPCXpresso.
For 30 Euro you get everthing you need to compile & debug.

Also it's easy to install and a lot of code samples are available.

Hope this helps,
Gerd
0 Kudos
Reply

961 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by igorsk on Mon Jun 28 04:09:55 MST 2010
You can program with any compiler that supports Cortex-M3/M0 (depending on your chip). However, the LPC-Link debug adapter currently works only with LPCXpresso IDE, and it seems NXP/codered/EA do not plan for this to change. You can, however, use another debug adapter if it supports SWD.
0 Kudos
Reply