Activate code not availible

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Activate code not availible

1,529件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sonia on Tue May 22 14:14:27 MST 2012
hello all;

I instaled LPCXpresso_4.0.6_152 but i have problem with activate code. in fact, when the instalation is complited and the devlop welcome page is opned i have his message :
[COLOR=red]Licence Type: UNACTIVATED(Activation not completed)
Debug limite:8k
Activation code : not availible [/COLOR]

I try with a other version LPCXpresso_4.1.0_190 but i have the same problem

in the tent of a response,
greetings,
0 件の賞賛
返信
6 返答(返信)

1,495件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jan 07 06:26:22 MST 2014
What is the URL of the page that you are trying to open?

The activation page is at:
http://www.lpcware.com/lpcxpresso/activate

You must be logged in to activate your product.
0 件の賞賛
返信

1,495件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fengshao1370 on Tue Jan 07 05:58:43 MST 2014
When I want to open the activate website,the website shows "You have attempted to access a page that doesn't exist."
0 件の賞賛
返信

1,495件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by researchinnovation on Wed May 23 00:31:23 MST 2012

Quote: Sonia
hello all;

I instaled LPCXpresso_4.0.6_152 but i have problem with activate code. in fact, when the instalation is complited and the devlop welcome page is opned i have his message :
[COLOR=red]Licence Type: UNACTIVATED(Activation not completed)
Debug limite:8k
Activation code : not availible [/COLOR]

I try with a other version LPCXpresso_4.1.0_190 but i have the same problem

in the tent of a response,
greetings,


Hi.. !!!
Open ur LPCxpresso IDE and go to "Help" and then "Product Activation" and click on "Create Serial Number and Activate" and you will get the serial number number on a small popped out window and fill the "open in external browser" and then register yourself on Code Red/Lpcxpresso and they will send you the activation code. [B]Help->product Activation->Create Serial number and activate.[/B]
Copy that code and paste on your [B]Help->Product Activation->Enter the Activation Code.[/B]

Hope this help.

Thanks & Regards....:)
0 件の賞賛
返信

1,495件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed May 23 00:12:11 MST 2012

Quote: Sonia

I instaled LPCXpresso_4.0.6_152 but i have problem with activate code. in fact, when the instalation is complited and the devlop welcome page is opned i have his message :
[COLOR=red]Licence Type: UNACTIVATED(Activation not completed)
Debug limite:8k
Activation code : not availible [/COLOR]



Have you actually gone through the LPCXpresso activation process? For more details, see section 3.3, "Activation" of the LPCXpresso Getting Started Guide. You can find this inside your product installation directory, or else from:

http://ics.nxp.com/lpcxpresso/#Support


If this doesn't get you going, then I suggest you post  exactly what steps you actually followed from installation onwards.

[ PS - the link Zero posted is incorrect for LPCXpresso users; this is a Red Suite specific FAQ ]

Regards,
CodeRedSupport
0 件の賞賛
返信

1,495件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sonia on Tue May 22 14:48:02 MST 2012

Quote: Zero
Why are you using old versions? Did you try to download an actual version?

Did you activate your version?

See: http://support.code-red-tech.com/CodeRedWiki/LicenseAndActivation



i can't
0 件の賞賛
返信

1,495件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue May 22 14:18:31 MST 2012
Why are you using old versions? Did you try to download an actual version?

Did you activate your version?

See: http://support.code-red-tech.com/CodeRedWiki/LicenseAndActivation
0 件の賞賛
返信