what this line of datasheet means?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what this line of datasheet means?

Jump to solution
1,699 Views
navidansari
Contributor III

hi

Untitled.png

it says other pins have limitation of VDD+.5 

what pins are other pins?

im using usart1 of lpc1768

can p2.1 recieve 5V signal and not break?

in what page of datasheet says it can or it can not?

Labels (1)
1 Solution
1,575 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the table 5(pin description) from the datasheet below:

http://www.nxp.com/docs/en/data-sheet/LPC1769_68_67_66_65_64_63.pdf 

In this table you can find a note about if this pin is 5v tolerant.

pastedImage_2.png

pastedImage_3.png

In addition please check the table 8. (static characteristics)

pastedImage_4.png

I hope this helps,


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,576 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the table 5(pin description) from the datasheet below:

http://www.nxp.com/docs/en/data-sheet/LPC1769_68_67_66_65_64_63.pdf 

In this table you can find a note about if this pin is 5v tolerant.

pastedImage_2.png

pastedImage_3.png

In addition please check the table 8. (static characteristics)

pastedImage_4.png

I hope this helps,


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,575 Views
navidansari
Contributor III

thanks allot

0 Kudos
Reply