what this line of datasheet means?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what this line of datasheet means?

ソリューションへジャンプ
1,658件の閲覧回数
navidansari
Contributor III

hi

Untitled.png

it says other pins have limitation of VDD+.5 

what pins are other pins?

im using usart1 of lpc1768

can p2.1 recieve 5V signal and not break?

in what page of datasheet says it can or it can not?

ラベル(1)
1 解決策
1,534件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the table 5(pin description) from the datasheet below:

http://www.nxp.com/docs/en/data-sheet/LPC1769_68_67_66_65_64_63.pdf 

In this table you can find a note about if this pin is 5v tolerant.

pastedImage_2.png

pastedImage_3.png

In addition please check the table 8. (static characteristics)

pastedImage_4.png

I hope this helps,


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,535件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the table 5(pin description) from the datasheet below:

http://www.nxp.com/docs/en/data-sheet/LPC1769_68_67_66_65_64_63.pdf 

In this table you can find a note about if this pin is 5v tolerant.

pastedImage_2.png

pastedImage_3.png

In addition please check the table 8. (static characteristics)

pastedImage_4.png

I hope this helps,


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,534件の閲覧回数
navidansari
Contributor III

thanks allot

0 件の賞賛
返信