what j5 connector has to be removed for flashing the embedded wizard code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what j5 connector has to be removed for flashing the embedded wizard code

1,448 次查看
suraj78725
Contributor I

hi, i am suraj,

why j5 connector has to be connected while dumping the code to the board via the mcuexpresso directly to access the gpio or common programs and removed while flashing the code via embedded wizard.

with regards 

suraj

0 项奖励
回复
4 回复数

1,391 次查看
suraj78725
Contributor I

hi zhang,

thanks for your response.

with regards

suraj

0 项奖励
回复

1,439 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Would be possible that you tell us the board that you are using or the device

 

Thanks

 

0 项奖励
回复

1,431 次查看
suraj78725
Contributor I

hi 

i am using lpc54628 nxp development board

thanks

0 项奖励
回复

1,399 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

J5 is Audio line input jack. It should not affect code download.

ZhangJennie_0-1609244840965.png

 

Is this issue related with a specific project or SDK demo code? or a common issue for all project?

Please specify how I can reproduce your issue on my side. I will check it.

 

Thanks,

Jun Zhang

 

0 项奖励
回复