what j5 connector has to be removed for flashing the embedded wizard code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what j5 connector has to be removed for flashing the embedded wizard code

1,557件の閲覧回数
suraj78725
Contributor I

hi, i am suraj,

why j5 connector has to be connected while dumping the code to the board via the mcuexpresso directly to access the gpio or common programs and removed while flashing the code via embedded wizard.

with regards 

suraj

0 件の賞賛
返信
4 返答(返信)

1,500件の閲覧回数
suraj78725
Contributor I

hi zhang,

thanks for your response.

with regards

suraj

0 件の賞賛
返信

1,548件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Would be possible that you tell us the board that you are using or the device

 

Thanks

 

0 件の賞賛
返信

1,540件の閲覧回数
suraj78725
Contributor I

hi 

i am using lpc54628 nxp development board

thanks

0 件の賞賛
返信

1,508件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

J5 is Audio line input jack. It should not affect code download.

ZhangJennie_0-1609244840965.png

 

Is this issue related with a specific project or SDK demo code? or a common issue for all project?

Please specify how I can reproduce your issue on my side. I will check it.

 

Thanks,

Jun Zhang

 

0 件の賞賛
返信