video on lpc1788. Is it possible?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

video on lpc1788. Is it possible?

974件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by siriasis on Sun Mar 11 16:47:26 MST 2012
Guys, Is it possible to run video on LPC1788. 15fps. Has anyone tried anything like this on this chip. Video information will come from external networking camera.

Thanks in advance
ラベル(1)
0 件の賞賛
返信
1 返信

948件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Sun Mar 11 18:45:36 MST 2012
You'll need to provide more information to offer a meaningful answer to that question.  It depends on the width of your memory (16 or 32-bit), the size of your LCD (320x240 isn't very demanding, but 800x480 is very taxing on the system), the screen refresh rate and not just the video framerate.

If you are using a 320x240 LCD and 320x240 video, it may be possible, but there are far to many variables involved to be able to provide a useful answer on if it's possible or not.
0 件の賞賛
返信