secure boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

secure boot

6,719件の閲覧回数
vannius
Contributor I

Hi,

I use secure boot as follows:

1、Generate four sets of certificates;serial number field of image certificates :3C:C3:00:00:AB:AB:AB:AB

2、with elftosb_gui, config load address to be 0x10000000; elftosb_gui show “Verifysignature ” is "success".

3、load  this  signed image;

4、config  "Version" of CFPA to 0x01 and config "ROTKH_REVOKE"为0x55; CFPA is attached;

5、config ROTKH of CMPA with RKTH generated by elftosb_gui;config SECURE_BOOT_CFG of CMPA to 0x40000000(signed image); DIGEST of CMPA is not configed。

after reset, the image is not right running。 why?

Can you provide an available certificate?   I suspect there is something wrong with my certificate。

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

6,263件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello 宁 解 ,

Please provide the certificate configuration file (.ext) .

BR

Alice

0 件の賞賛
返信

6,263件の閲覧回数
vannius
Contributor I

hello,Alice:

OpenSSL I haven't yet configured successfully,so certificates are generated by a tool found online; I'm trying to configure OpenSSL. Certificate in SDK expired and elftosb reported an error,Is it possible to provide a certificate?

   other question, DIGEST of CMPA is not configed,secure boot is configed; Is there any other way to modify CMPA except bootloader.

   I find that IMAGE_KEY_REVOKE of CFPA  has 4 bytes from address  0x9DE10,  but it only need two bytes; so i shall write 3C C3 00 00 from  address 0x9DE10 ? 

  Can you provide an example of a complete set of operational processes?  What is the first step?What is the second step? ...

0 件の賞賛
返信

6,263件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ning xie,

About the steps, please refer to this Application Note:

https://www.nxp.com/docs/en/application-note/AN12283.pdf    

0 件の賞賛
返信

6,263件の閲覧回数
vannius
Contributor I

Hello,Alice:

Thank you very much for your reply;The following three questions can be answered:

1、OpenSSL I haven't yet configured successfully,so certificates are generated by a tool found online; I'm trying to configure OpenSSL. Certificate in SDK expired and elftosb reported an error,Is it possible to provide a certificate?

 

 2、 DIGEST of CMPA is not configed,secure boot is configed; Is there any other way to modify CMPA except bootloader.

 

  3、 I find that IMAGE_KEY_REVOKE of CFPA  has 4 bytes from address  0x9DE10,  but it only need two bytes; so i shall write 3C C3 00 00 from  address 0x9DE10 ? 

0 件の賞賛
返信

6,263件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ning xie,

1. Sorry I can't give you a certificate, as I also need give you the Key. What's the problem when you using OpenSSL?

2. About this question, I will help you ask development team whether this is method.

3. From  AN12283 we can see, in IMAGE_KEY_REVOKE, the 31:16 reserved, only two bytes (15:0) are used as

IMG revocation counter:

pastedImage_1.png

0 件の賞賛
返信

6,263件の閲覧回数
vannius
Contributor I

Hello,Alice:

 

Thank you very much for your reply;When I use boot, I do the following:

Data preparation process:

1、I generated a secure image with a starting address of 0x10000000,  the size of this image is 0x10424;  config of this image :load address(0x10000000) 、imageTZ-M Enable but no preset data、add four ROOT keys, key is generated by referring to AN12283_LPC55Sxx_Secure_boot; As an annex“elftosb_gui”

   The starting address of the  non secure code is 0x20000, no crc 、no signed;

2、CFPA:config  "Version" of CFPA to 0x01 and config "ROTKH_REVOKE"为0x55;As an annex“cfpa_9DE00_1.bin”

3、CMPA is generated using elftosb_gui tool: SECURE_BOOT_CFG(0x9E41C) is Boot signed images、

RKTH is generated using elftosb tools(01747922a5d76949d3db0b7eb1cce7cfce9a46516456b19ea78f53375af2b943)、

DIGEST also is generated using elftosb tools.As an annex“cmpa_9E400_1.bin”

 note: puf、prince are not used.

Operating process:

   1、 Enter boot,erase flash :blhost.exe -p COM45 -- flash-erase-region 0x00000 0x40000; 

2、load image:blhost -p COM45 write-memory 0x20000 hello_world_ns_0614.bin 、blhost -p COM45 write-memory 0 hello_world_s_sig_0614.bin;

3、read and write CFPA :

     

blhost -p COM45 read-memory 0x9DE00 512 cfpa_9DE00_0.bin
blhost -p COM45 read-memory 0x9E000 512 cfpa_9E000_0.bin
blhost -p COM45 read-memory 0x9E200 512 cfpa_9E200_0.bin


blhost -p COM45 write-memory 0x9DE00 cfpa_9DE00_1.bin


blhost -p COM45 read-memory 0x9DE00 512 cfpa_9DE00_2.bin
blhost -p COM45 read-memory 0x9E000 512 cfpa_9E000_2.bin
blhost -p COM45 read-memory 0x9E200 512 cfpa_9E200_2.bin

4、read and write CMPA :

  

blhost -p COM45 read-memory 0x9E400 512 cmpa_9E400_0.bin

blhost -V -p COM45,57600 -- write-memory 0x9E400 cmpa_9E400_1.bin

5、reset,Running error;

 

these steps are  right ? Looking forward to your reply.

0 件の賞賛
返信