LPC1768 ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 ADC

1,711 Views
rajeshsdave
Contributor I

I am using 12 BIT ADC of LPC17xx Series. In the User Manual of LPC17xx very little information is available about Using ADC. Where can I find More info Like ADC Internal Block Diagram,Its Clock Selection and Interrupt Mechanism?

Labels (1)
0 Kudos
Reply
1 Reply

1,584 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi RAJESH DAVE

Please refer doc/code in this package:

https://www.nxp.com/docs/en/application-note/AN10974_-_LPC176x_175x_12-bit_ADC_design_guidelines.zip 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply