read & write SRAM OM2NTP5332

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

read & write SRAM OM2NTP5332

1,362 次查看
StefanC
Contributor I

Hello,

I have been trying to read and write SRAM data using the LPC55S69 pass through example provided here: example. The program it selves works, no errors and warnings occur and the green LED turns on when an NFC device is nearing. But when trying to simply send/read data I can only acces the EEPROM memory and not the SRAM, is there a specific app that is needed or is something else not properly setup?

thanks!

 

PS. SW3 3-4 is set to on for the VCC and sw6 is set to 5V. 

0 项奖励
回复
1 回复

1,317 次查看
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir, I'm very sorry for not answering you back regarding your case.

Could you please let me know if you are using our NTAG 5 Android App or a custom one?

According to Section 6 of AN12364, it is required to configure the Arbiter mode to SRAM Pass-Through mode, please be sure you are following these recommendations.

Again, I'm very sorry for not answering earlier sir. Please accept our apology.

Best Regards,
Fabian
0 项奖励
回复