Hello Jun Zhang
1. SDK version is: 2.82(376 2020-08-19)
2. I tried creating different projects & workspaces. But it doesn't work properly.
3. I tried it on a different PC with the same project & board. It works completely fine.
4. I haven't tried it. I am using LCP55S69 JBD64 TR7UC409.000 02
5. I already tried that solution and updated firmware. But the error is still there. It couldn't fix the error.
Update: The main problem is it can find the probe but can't connect to it. Error is still there, but there is a time I can connect to the board from my pc. The walkthrough is like this:
- Connect the board to PC and power supply
- Start MCUXpresso and start debugging
- Open probe error will occur
- Close MCUXpresso and every open application
- Restart your PC
- Do not disconnect the board from the PC and power supply.
- Open MCUXpresso and connect to the board
- It will connect
Is there any solution that I can connect the board normally? Like, not restarting my PC or not closing MCUXPresso.
Have a nice day
Khos-Erdene