"Nand Flash Not Found Error" while loading S1l in lpc3250

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"Nand Flash Not Found Error" while loading S1l in lpc3250

1,754件の閲覧回数
satishpandey
Contributor I


we are using custom Board of Lpc 3250 with similar configuration as suggested board like EA/Phytech of SLC Nand flash with LPC 3250 .

 

while we attempt to load S1 Loader using LPC3250 Loader Utility using uart file transfer's successfully but aftre transfer complete when we enable terminal message appears displaying "nanad Flash not found "   / "nand Flash Could not initialise"  / "Could not erase "  ....etc

 

please suggest remedy of such problem

タグ(1)
1 返信

1,385件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You could take a look at the following links that provide related information:

Restoring the Stage 1 Loader in NAND Flash

Writing to NAND Flash on Phytec LPC3250 board

PHY3250 boot loaders

In case that nothing helps, it may be recommended directly contacting Phytech.

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------