Please provide schematic symbol for LPC4370FET256 in orcad 10.5 format

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Please provide schematic symbol for LPC4370FET256 in orcad 10.5 format

877 Views
sujayp
Contributor II

These microcontroller have very complicated schematic symbols and creation takes lots of time and is error prone.

 

please will any one provide schematic symbol for LPC4370FET256 in orcad 10.5 format

thanks - - - - would be nice if you would provide a location where it is possible to down load the schematic symbols

 

Sujay  P

iFuture Systems

+917760274808

Labels (1)
Tags (1)
3 Replies

603 Views
soledad
NXP Employee
NXP Employee

Hi,

Attached you will find the Orcad Symbols for the LPC18xx and LPC43xx

I hope this helps!


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

603 Views
ajeeshsahadevan
Contributor I

Hi,

I am also looking for LPC4357FET256 orcad capture symbol.

Kindly help me to download this symbol.

Thanks in advance

Ajeesh

0 Kudos
Reply

603 Views
soledad
NXP Employee
NXP Employee

Hi, Ajeesh,

The attachments are for LPC43XX series.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply