question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

question

1,231件の閲覧回数
milan021
Contributor I

Hello,

I have microcontroller LPC5512JBD100E on my board, I have to check if the USB cable is connected with the board, and to have feedback from the controller about that. Which software do I need to have and how to do it ?

Best regards,

Milan

0 件の賞賛
返信
1 返信

1,207件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the LPC5512 has one full-speed USB, which can function as both device and host.

We provide USB stack in SDK package, you can download SDK package from the link:

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-s...

You can select the USB class example in SDK USB example for example CDC, MSC...

From hardware perspective, when the USB of LPC5512 functions as a device, when a USB cable is inserted, an USB interrupt will be fired on LPC5512 side, the host can communicate with the device and exchange the descriptor inf.

Hope it can help you

BR

XiangJun

0 件の賞賛
返信