play a audio file stored in sdcard using lpc54608 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

play a audio file stored in sdcard using lpc54608 ?

974件の閲覧回数
pylaramesh
Contributor I

  i want to play a audio file stored in sdcard ? is any funtions are there in fats?

ラベル(1)
0 件の賞賛
返信
1 返信

851件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

No, unfortunately there is no a funtion like you need. It is necessary to create your own algorithms. 

Please check the AN11855 application note, this appnote explains the advantages of the LPC5411x ARM Cortex-M4F microcontroller family for a product which requires voice detection and voice recognition features.

https://www.nxp.com/docs/en/application-note/AN11855.zip 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信