new created project file is not working on my lpc board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

new created project file is not working on my lpc board

1,156件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chethan kumar on Tue Jul 29 01:37:59 MST 2014
Hi,

i am new to lpcexpresso IDE,I have installed LPCXpresso v6.1.4_194 tool and i want to work on FreeRTOS so i get the lpc1768 source example from freertos.org attached here that zip file and  also when i am going to use that examples and within that example main.c file i can change the code  build it and burn to my lpc board its is working fine but when i go to create new project, build it and burn to my lpc board it wont response may be problem in creating new project i don't exactly but main.c code same in both project,even i didn't get  led blinking  through gpio also.

i hope u understand my problem and please give me the solution

thank u in advance for your reply.....


Regards,

chethan kumar

Original Attachment has been moved to: source-code-for-LPC17xx-examples.rar

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,116件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chethan kumar on Wed Jul 30 00:12:35 MST 2014

Hi,
    Thanks for your reply....
  I changed IDE version as per you are mentioned above in this version i couldn't work with lpc examples also (attached .rar file above). and i worked on LPCOPEN example freertos_blinky porject i didnt get any result. previous version IDE what i said everything is fine (if i work within the example project)only the problem is when i go to create ne project it wont work but in this version i didn't get the result with even examples also.



Regards,

chethan kumar
0 件の賞賛
返信

1,116件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jul 29 03:16:53 MST 2014
Get LPCXpresso 7.30 :
[list]
  [*]http://www.lpcware.com/lpcxpresso/download
[/list]
Download LPCOpen for LPC17xx from :
[list]
  [*]http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc17xx-packages
[/list]

And try using the FreeRTOS example include as part of LPCOpen.

I would also strongly suggest that before you go any further, you read the LPCXpresso User Guide, and watch the "Rapid Embedded Development…" video at:

http://www.lpcware.com/lpcxpresso

Regards,
LPCXpresso Support
0 件の賞賛
返信