missing exposed pad at LPC5516JBD100 layout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

missing exposed pad at LPC5516JBD100 layout

ソリューションへジャンプ
1,492件の閲覧回数
username5000
Contributor I

Hi,

after downloading the BXL file for the LPC5516JBD100, I noticed that the pad for GND under the uC is missing in the layout.

The general pads for the pins were also tight when compared to the suggested data from the data sheet.

Since this has unsettled me, I ask for a short feedback.

Note: I exported the file to Altium using the Ultra Librarian program.

Thank you for your feedback

0 件の賞賛
返信
1 解決策
1,478件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls go to the link and download the latest data sheet of LPC5516JBD100.

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

You can draw the schematics library for the LPC5516JBD100 based the signal assignment on the data sheet. The data sheet is correct, if the BXL does not match with data sheet, pls use data sheet as correct one.

 

Hope it can help you

BR

XiangJun Rong

 

 

元の投稿で解決策を見る

1 返信
1,479件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls go to the link and download the latest data sheet of LPC5516JBD100.

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

You can draw the schematics library for the LPC5516JBD100 based the signal assignment on the data sheet. The data sheet is correct, if the BXL does not match with data sheet, pls use data sheet as correct one.

 

Hope it can help you

BR

XiangJun Rong