missing exposed pad at LPC5516JBD100 layout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

missing exposed pad at LPC5516JBD100 layout

Jump to solution
1,494 Views
username5000
Contributor I

Hi,

after downloading the BXL file for the LPC5516JBD100, I noticed that the pad for GND under the uC is missing in the layout.

The general pads for the pins were also tight when compared to the suggested data from the data sheet.

Since this has unsettled me, I ask for a short feedback.

Note: I exported the file to Altium using the Ultra Librarian program.

Thank you for your feedback

0 Kudos
Reply
1 Solution
1,480 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls go to the link and download the latest data sheet of LPC5516JBD100.

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

You can draw the schematics library for the LPC5516JBD100 based the signal assignment on the data sheet. The data sheet is correct, if the BXL does not match with data sheet, pls use data sheet as correct one.

 

Hope it can help you

BR

XiangJun Rong

 

 

View solution in original post

1 Reply
1,481 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls go to the link and download the latest data sheet of LPC5516JBD100.

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

You can draw the schematics library for the LPC5516JBD100 based the signal assignment on the data sheet. The data sheet is correct, if the BXL does not match with data sheet, pls use data sheet as correct one.

 

Hope it can help you

BR

XiangJun Rong